2.5.3 Configuring the Library

The application designer must specify the following configuration parameters while using the CDC Function Driver. The configuration macros that implement these parameters must be located in the system_config.h file in the application project and a compiler include path (to point to the folder that contains this file) should be specified.

Macros

Name Description
USB_DEVICE_CDC_INSTANCES_NUMBER Specifies the number of CDC instances.
USB_DEVICE_CDC_QUEUE_DEPTH_COMBINED Specifies the combined queue size of all CDC instances.
Configuration on MCCThis section describes the symbols available in the MCC that can be configured.