1.15 PORT Polling
This example application demonstrate how to poll the switch input, and indicate the switch status using the LED.
Description
This application uses the PORT Peripheral library to read the GPIO pin connected to the switch, and drives the GPIO pin connected to the LED to indicate the switch status. LED is turned ON when the switch is pressed and turned OFF when the switch is released.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/port/port_led_on_off_polling/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sam_l22_xpro.X | MPLABX project for SAM L22 Xplained Pro Evaluation Kit |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sam_l22_xpro.X | SAM L22 Xplained Pro Evaluation Kit |
Setting Up SAM L22 Xplained Pro Evaluation Kit
- Connect the Debug USB port on the board to the computer using a micro USB cable
Running the Application
- Build and Program the application using its IDE.
- LED is turned on when the switch is pressed and turned off when the switch is released.
| Board | Switch Name | LED Name |
|---|---|---|
| SAM L22 Xplained Pro Evaluation Kit | SW0 | LED0 |