1.3.8 SAM9X60-Curiosity board: Building and Running the UART Bootloader with NAND Flash media applications

Downloading and building the application

To clone or download this application from Github,go to the main page of this repository and then click Clone button to clone this repo or download as zip file. This content can also be download using content manager by following these instructions

Path of the application within the repository is apps/mpu_uart_bootloader/

To build the application, refer to the following table and open the project using its IDE.

Bootloader Application

Project NameDescription
bootloader_nand_flash/firmware/sam_9x60_curiosity.XMPLABX Project for SAM9X60-Curiosity board

Test Application

Project NameDescription
test_app/firmware/sam_9x60_curiosity.XMPLABX Project for SAM9X60-Curiosity board

Setting up SAM9X60-Curiosity board

  • Connect the USB port J1 on board to the computer using a micro USB cable (to power the board)

  • Connect the J11 on board to the computer using a UART-FTDI cable (to enable debug com port)

  • Short NAND BOOT J4 jumper

Setting up the host script

Running the Application

  1. Open the test application project test_app/firmware/sam_9x60_curiosity.X in the IDE

  2. Build the project to generate the harmony.bin binary (Do not program the binary)

  3. Open the bootloader project bootloader_nand_flash/firmware/sam_9x60_curiosity.X in the IDE

  4. Build the project to generate the harmony_bootloader.bin binary (Do not program the binary)

  5. Download and unzip SAM-BA

  6. Open the command prompt and change the current directory to <harmony3_path>/bootloader_apps_uart/deps/at91bootstrap_binaries_sam_9x60_curiosity/nand_flash/ and run the below command

     <sam-ba_path>/sam-ba.exe -p serial -b sam9x60-ek -a nandflash:::0xc2605007 -c erase::0x40000 -c writeboot:boot.bin

    Note - Here sam9x60-ek board is used as SAM-BA support is not available on SAM9X60-Curiosity board on SAM-BA v3.7

  7. Change the current directory to <harmony3_path>/bootloader_apps_uart/apps/mpu_uart_bootloader/bootloader_nand_flash/firmware/sam_9x60_curiosity.X/dist/sam_9x60_curiosity/production/ and run the below command

     <sam-ba_path>/sam-ba.exe -p serial -b sam9x60-ek -a nandflash:::0xc2605007 -c erase:0x40000:0x80000 -c write:harmony_bootloader.bin:0x40000
  8. Reset or Power cycle the device. GREEN LED will be turned-on to indicate that harmony bootloader code is running on the target

  9. Run the btl_host.py from command prompt to program the application binary

     python <harmony3_path>/bootloader/tools/btl_host.py -v -i <COM PORT> -d sam9x6 -p 4096 -f <harmony3_path>/bootloader_apps_uart/apps/mpu_uart_bootloader/test_app/firmware/sam_9x60_curiosity.X/dist/sam_9x60_curiosity/production/harmony.bin
  10. Following snapshot shows output of successfully programming the test application

    • Rebooting and Reboot Done messages in below output signifies that bootloading is successful

    output
  11. If above step is successful then the GREEN LED should start blinking

  12. Open the Terminal application (Ex.:Tera Term) on the computer

  13. Configure the serial port settings as follows:

    • Baud : 115200

    • Data : 8 Bits

    • Parity : None

    • Stop : 1 Bit

    • Flow Control : None

  14. Reset or Power cycle the device

  15. GREEN LED should start blinking and you should see below output on the console

    output
  16. Press and hold the Switch USER and then press Reset button or Power cycle the device to force trigger bootloader at startup

  17. Repeat Steps 9-15 once

    • This step is to verify whether bootloader is triggered by switch press at reset

Additional Steps (Optional)