1.3 MPU UART Bootloader
This example application shows how to use the Harmony Bootloader to bootload an application from SD/eMMC/NAND/Serial flash memory and receives new application image using UART protocol and write it to SD/eMMC/NAND/Serial flash memory.
Bootloader Application
This is a bootloader application which resides from
Bootloader stored into SD/eMMC/NAND/Serial flash memory
Bootloader executes from DDR memory. AT91Bootstrap loads bootloader from SD/eMMC/NAND/Serial flash memory to DDR memory and executes it
It uses the DBGU Com port of the device to receive application binary from host PC
It calls the bootloader_Tasks() function which receives application to be programmed into SD/eMMC/NAND/Serial flash memory over UART channel. And it loads application image from SD/eMMC/NAND/Serial flash memory to DDR memory and executes it
It turns on an LED
Trigger Methods
- It uses the On board Switch as bootloader trigger pin to force enter the bootloader at reset of device
Test Application
This is a test application which resides from
- Application stored into SD/eMMC/NAND/Serial flash memory
It will be loaded from SD/eMMC/NAND/Serial flash memory to DDR memory by bootloader application and starts application execution
It blinks an LED and provides console output
Development Kits
The following list provides links to documentation on how to build and run UART bootloader on different development kits