1 MPLAB® Harmony Bootloader Application Examples for UART
MPLAB® Harmony is an extension of the MPLAB ecosystem for creating embedded firmware solutions for Microchip 32-bit SAM and PIC® microcontroller and microprocessor devices.
This repository contains the MPLAB Harmony 3 UART Bootloader application examples.
Bootloader Library
Refer to the Bootloader Library Help for understanding:
- Bootloader framework
- How the Bootloader library works
- Bootloader library configurations
- Bootloader memory layout
Bootloader Examples
The following applications are provided to demonstrate the UART bootloader.
| Name | Description |
|---|---|
| UART Bootloader | This example application shows how to use the Bootloader Library to bootload an application using UART protocol |
| UART Fail Safe Bootloader | This example application shows how to use the Bootloader Library to bootload an application on device having dual Flash bank feature using UART protocol |
| MPU UART Bootloader | This example application shows how to use the Harmony Bootloader to bootload an application from SD/eMMC/NAND/Serial Flash memory and receives new application image using UART protocol and write it to SD/eMMC/NAND/Serial Flash memory |