1.3 MPU UART Bootloader

This example application shows how to use the Harmony Bootloader to bootload an application from SD/eMMC/NAND/Serial Flash memory and receives new application image using UART protocol and write it to SD/eMMC/NAND/Serial Flash memory.

Bootloader Application

  • This is a bootloader application which resides from:

    • Bootloader stored into SD/eMMC/NAND/Serial Flash memory

    • Bootloader executes from DDR memory. AT91Bootstrap loads bootloader from SD/eMMC/NAND/Serial Flash memory to DDR memory and executes it.

  • It uses the DBGU Com port of the device to receive application binary from host PC

  • It calls the bootloader_Tasks() function which receives application to be programmed into SD/eMMC/NAND/Serial Flash memory over UART channel. And it loads application image from SD/eMMC/NAND/Serial Flash memory to DDR memory and executes it.

  • It turns on an LED

  • Trigger methods:

    • It uses the On board Switch as bootloader trigger pin to force enter the bootloader at reset of device

Test Application

  • This is a test application which resides from:

    • Application stored into SD/eMMC/NAND/Serial Flash memory
  • It will be loaded from SD/eMMC/NAND/Serial Flash memory to DDR memory by bootloader application and starts application execution

  • It blinks an LED and provides console output