2.4 LEDs

All LEDs are mounted on the top side of the board.

The table below provides an overview of the LEDs and the states they signal.

Table 2-3. LEDs
NameStateDescriptionNote
PWROffThe EVB-LAN8670-USB-D is not powered.—
On (green)The EVB-LAN8670-USB-D is powered.
LED1OffFuture use
On (red)
LED2OffThe EVB-LAN8670-USB-D does not send or receive data.

It is recommended to use the latest Windows® or Linux® driver, which can be found

at: www.microchip.com/en-us/development-tool/EV62B92A

Blinking (yellow)The EVB-LAN8670-USB-D sends or receives data.
LED3OffFuture use—
On (green)
LSOffNetwork link is down.
On (green)Network link is up.