5.1 FAQs and Tips
1. How can the user change the Wi-Fi configuration?
- Connect to the USB and click the
‘
click-me’ file to reach the dedicated www.avr-iot.com/avr-iot/gcp page for the device and enter the new credentials in the web form. Download the resulting file to the CURIOSITY drive. Read more in Section Via AVR-IoT Webpage. - Connect to the USB and open a
serial port terminal (Windows users will need to install serial port drivers).
From the command line, use the
Wi-ficommand. Read more in Section Via AVR-IoT Webpage. - Press the SW0 button while powering up the board and the WINC will turn to Access Point mode. Connect the laptop or phone to it and fill in the online form. See Section Connecting the Board to Wi-Fi® Networks for details.
- Use MCC to re-build the project after changing the default Wi-Fi configuration in the WINC module. Reprogram the board using MPLAB X or drag and drop the new image to the CURIOSITY drive. Further details can be found in Section Code Generation from MCC .
2. How can the user change the Wi-Fi credentials using the online form without exposing the details to security threats?
Although it appears in the browser, the Wi-Fi credential setup form does not transfer any information to third parties. A small text file (WIFI.CFG) is created (this can also be done manually using any text editor) and it is recommended that saves it directly to the CURIOSITY drive. Since the browser settings vary according to the platform and personal preferences, the user might have to change them or perform a drag and drop from the default download folder. Even though it looks like the WIFI.CFG file is now stored on the CURIOSITY drive, this is just an artifact of the operating system (caching). No file is permanently recorded and the information contained is immediately used to update the Wi-Fi module settings. These settings will be maintained after subsequent power cycles of the AVR-IoT Development Board, but the file will disappear.
3. Can a phone/tablet alone be used to perform the demo?
Assuming the user has a way to provide power to the board (a USB back up battery, a USB charger, a Li-Ion battery, or other 3.3V-5V power supply), the QR code can be scanned (on a sticker under the board, next to the Microchip and Google color logos) using any smartphone camera (old operating system versions might still require a separate app) and open the resulting link in the smartphone browser.
4. The user scanned the bar code with the phone/tablet, but nothing happened?
Ensure the scanning of the QR code present on the sticker under the AVR-IoT WG board. It can be recognized by the distinguishing squares on the three of its corners and its proximity (same sticker) to the MCHP and Google logos (in color). Although there are also other bar codes present on the Wi-Fi module, and/or the anti-static bag the board came with, those are not QR codes.
5. Which battery is recommended to be used with the AVR-IoT WG Sensor Node board?
Microchip recommends Li-Ion or Li-Poly batteries with at least 400 mAh capacity and 3.7V nominal. For more information about powering the board, refer to the AVR-IoT Wx Hardware User Guide.
Other Helpful Tips:
The following steps are not required for operating the AVR-IoT WG Sensor Node board, but will significantly increase the possibility of positive results.
- Get a USB cable with all the four wires connected. There are a lot of non-compliant USB cables available that provide only 5V power (two wires). How can the user verify it? Plug the board into the laptop and check in the File Manager (Finder) for the presence of a new hard drive (named CURIOSITY). If it fails to pop up after a second or two, the cable is not the appropriate one.
- Prepare the Wi-Fi router for the demo. The easiest way to go is to set up the phone as a hotspot. The following credentials should be used, name (SSID): MCHP.IOT and password: microchip (WPA 2 is assumed, do no use WEP nor OPEN.) This Wi-Fi configuration is the factory default for all boards, so it will minimize the effort for first-time users. If preparing for a (medium/large) classroom demo, the user should set up a proper Wi-Fi router (2.4 GHz) instead. This will give a better range and capacity while using the same Wi-Fi credentials, if possible.
- Make Google Chrome or Firefox the default web browser. Safari works well on MACs. Internet Explorer is not recommended.
- Ensure no pop-up blockers or other anti-virus browser extensions are active. These can and will interfere with the script that is at the heart of the www.avr-iot.com/ microsite. Often, these can be selectively disabled for that specific webpage.
- Take into account the amount of Wi-Fi pollution in the place where the board is operated.
- If using a router, verify that the network does not have a firewall that can block access to the Google Cloud server. If using a mobile 4G (or phone LTE hotspot) for Internet connectivity, ensure it is fully charged and does not have any firewall settings that might block access.