2.1 Connecting the Board to the Host PC
The AVR-IoT WG development board can be connected to a computer using a standard Micro-USB cable. Once plugged in, the LED array at the top right-hand corner of the board should flash twice in the following order: Blue, Green, Yellow, and Red. When the board is not connected to Wi-Fi , the blue LED will blink continuously. The board will appear as a Removable Storage Device on the host PC, as shown in Curiosity Board as Removable Storage. Double click the CURIOSITY drive to open it and get started.
- CLICK-ME.HTM – redirects the user to the AVR-IoT web demo application
- KIT-INFO.HTM – redirects the user to a site containing information and resources about the board
- KIT-INFO.TXT – a text file with details about the PKOB nano firmware and the board’s serial number
- PUBKEY.TXT – a text file with the public key used for data encryption
- STATUS.TXT – a text file with the status of the board
Double click on the CLICK-ME.HTM file to enter the dedicated webpage to access the web application.