1.1 ADC DMA mode
This example application shows how to couple the ADC and the XDMAC peripherals to automatically transfer the data conversion of an analog input into internal memory. After the DMA transfer, the results of the converted samples are printed to the console.
Description
In this example, Analog input voltage in the range of 0 V to 3.3 V (from potentiometer) is fed to the ADC and converted value is displayed on the console. The ADC conversion is triggered once in freerun mode and XDMAC transfers are started every seconds to capture a set of samples.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/adc/adc_dma_mode/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| adc_dma_mode_sam_rh707_ek.X | MPLABX project for SAM RH707F18 Evaluation Kit |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| adc_dma_mode_sam_rh707_ek.X | SAM RH707F18 Evaluation Kit |
Setting Up SAM RH707F18 Evaluation Kit
- Connect the Debug USB port on the board to the computer using a micro USB cable
- Connect the J1 (USB-C) port on the board to the computer using a USB-C cable
Running the Application
- Open the Terminal application (Ex.:Tera term) on the computer
- Connect to the USB to UART COM port and configure the serial settings as
follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
- Build and Program the application project using its IDE
- Reset the board to run the application
- Vary ADC input voltage from
potentiometer (R109 - POT) and observe ADC input sample in voltage on
console