1.9 FLEXCOM USART Blocking
This example application shows how to use the FLEXCOM module in USART mode.
Description
This application configures the FLEXCOM peripheral in USART mode and performs read and write operation in a blocking manner. The CPU polls the peripheral register continuously to manage the transfer. It receives a line of characters from the terminal window and echoes them back.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/flexcom/flexcom_usart_echo_blocking/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sam_rh707_ek.X | MPLABX project for SAM RH707F18 Evaluation Kit |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sam_rh707_ek.X | SAM RH707F18 Evaluation Kit |
Setting Up SAM RH707F18 Evaluation Kit
- Connect the Debug USB port on the board to the computer using a micro USB cable
- Connect the debugger probe to J5 connector
- Connect the J1 (USB-C) port on the board to the computer using a USB-C cable
Running the Application
- Open the Terminal application (Ex.:Tera term) on the computer
- Connect to the USB to UART COM port and configure the serial settings as
follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
- Build and Program the application using its IDE
- The console displays the following message

- Type a line of characters and press the Enter keyNote: Number of characters entered before pressing enter key must be less than 256.
- Entered line will be echoed back and the LED is toggled
- The following table provides the LED name:
Board LED Name SAM RH707F18 Evaluation Kit LED0