m_ZBPeripheral?.ZBConnectionDelegate = self
/// A protocol that provides the peripheral connection related information.
public protocol ZBProvisionConnectionDelegate {
/// Tells the delegate that discovered a peripheral while scanning for devices.
/// - Parameters:
/// - peripheral: The discovered peripheral.
/// - deviceName: The name of peripheral.
/// - rssi: The current received signal strength indicator (RSSI) of the peripheral, in decibels.
/// - isConnectable: To indicates the peripheral is connectable or not.
func didDiscoverPeripheral(peripheral: CBPeripheral,deviceName: String,rssi:NSNumber, isConnectable:Bool)
/// Tells the delegate that connected to a peripheral.
func didConnected()
/// Tells the delegate that disconnected from a peripheral.
func didDisconnected()
}
//scan for peripheral
m_ZBPeripheral?.startScan()
//stop scan
m_ZBPeripheral?.stopScan()
//connect peripheral
m_ZBPeripheral?.connectPeripheral(peripheral)
//disconnect current connected device
m_ZBPeripheral?.disconnectPeripheral()
Scan: to
discover the nearby Bluetooth Low Energy Provisioning
devices.Figure 1-19. Scanning Process
Connection: to connect/disconnect the Bluetooth Low
Energy Provisioning devices.Figure 1-20. Connection Process
Device Information and
Provision Control:
Implement the
delegate.
m_ZBPeripheral?.ZBDelegate = self
/// A protocol that provides updates for the provisioning services status.
public protocol ZBProvisionResponseDelegate {
//func didDisconnected()
/// Tells the delegate that retrieving the device type.
/// - Parameter type: Device type of peripheral.
func updateDeviceType(type:UInt8)
/// Tells the delegate that retrieving the device name.
/// - Parameter name: The device name of peripheral.
func updateDeviceName(name:String)
/// Tells the delegate that retrieving the software version.
/// - Parameter version: The software version of peripheral.
///
/// The software version is up to 16 bytes.
func updateSWVersion(version:Data)//up to 16 bytes
/// Tells the delegate that retrieving the channel mapping.
/// - Parameter channel: The channel mapping of peripheral.
func updateChannelMap(channel:Data)//4 bytes
/// Tells the delegate that retrieving the current channel.
/// - Parameter channel: The current channel of peripheral.
func updateCurrentChannel(channel:UInt8)
/// Tells the delegate that retrieving the device state.
/// - Parameter state: The device state of peripheral.
func updateDeviceState(state:UInt8)
/// Tells the delegate that retrieving the MAC ID.
/// - Parameter id: The MAC ID of peripheral.
func updateMACID(id:Data)//8bytes
/// Tells the delegate that retrieving the light mode from peripheral.
/// - Parameter mode: The light mode of peripheral.
func updateLightMode(mode:UInt8)
/// Tells the delegate that the channel update successfully.
func didUpdateChannel()
/// Tells the delegate that the device name update successfully.
func didUpdateDeviceName()
/// Tells the delegate that the update status of commission process.
/// - Parameter status: The commission upddate status.
func didCommission(status:UInt8)
/// Tells the delegate that the commission process is started.
func didStartCommission()
/// Tells the delegate that retriving an error when sending the command.
/// - Parameters:
/// - ID: The command ID.
/// - errorCode: The error code.
///
/// Please refer to the ZB_COMMISSION_COMMAND_ID and ZB_COMMISSION_COMMAND_ID2 for the command ID.
/// Please refer to the ERROR_CODE for error code definition.
func errorResponse(ID:UInt8,errorCode:UInt8)
/// Updates the stack type with the given status.
/// - Parameter status: The status to update the stack type with.
func updateStackType(status: UInt8)
/// Updates the channel mask with the given data.
/// - Parameter data: The data to update the channel mask with.
func updateChannelMask(data: Data)
/// Updates the PAN ID with the given data.
/// - Parameter data: The data to update the PAN ID with.
func updatePanID(data: Data)
/// Updates the extended PAN ID with the given data.
/// - Parameter data: The data to update the extended PAN ID with.
func updateExtPanID(data: Data)
/// Updates the network name with the given name.
/// - Parameter name: The name to update the network name with.
func updateNetworkName(name: String)
/// Updates the network key with the given data.
/// - Parameter data: The data to update the network key with.
func updateNetworkKey(data: Data)
/// Updates the mesh local prefix with the given data.
/// - Parameter data: The data to update the mesh local prefix with.
func updateMeshLocalPrefix(data: Data)
/// Updates the user parameter with the given data.
/// - Parameter data: The data to update the user parameter with.
func updateUserParameter(data: Data)
/// Delegate method that handles the response after the app sends the SetExtPanID data to the BLE device.
/// This method is called when the BLE device sends back the set pan ID data response.
/// The response status indicates whether the operation was successful.
/// - Parameter status: A value indicating the response status (1 for failure, 0 for success).
func setPanIdResponse(status: UInt8)
/// Delegate method that handles the response after the app sends the SetExtPanID data to the BLE device.
/// This method is called when the BLE device sends back the set ext pan ID data response.
/// The response status indicates whether the operation was successful.
/// - Parameter status: A value indicating the response status (1 for failure, 0 for success).
func setExtPanIdResponse(status: UInt8)
/// Delegate method that handles the response after the app sends the setCurrentChannel data to the BLE device.
/// This method is called when the BLE device sends back the current channel data response.
/// The response status indicates whether the operation was successful.
/// - Parameter status: A value indicating the response status (1 for failure, 0 for success).
func setCurrentChannelResponse(status: UInt8)
/// Delegate method that handles the response after the app sends the SetChannelMask data to the BLE device.
/// This method is called when the BLE device sends back the channel mask data response.
/// The response status indicates whether the operation was successful.
/// - Parameter status: A value indicating the response status (1 for failure, 0 for success).
func setchannelMaskResponse(status: UInt8)
/// Delegate method that handles the response after the app sends the SetUserParameter data to the BLE device.
/// This method is called when the BLE device sends back the set user parameter data response.
/// The response status indicates whether the operation was successful.
/// - Parameter status: A value indicating the response status (1 for failure, 0 for success).
func setUserParameterResponse(status: UInt8)
/// Delegate method that handles the response after the app sends the SetNetworkName data to the BLE device.
/// This method is called when the BLE device sends back the set network name data response.
/// The response status indicates whether the operation was successful.
/// - Parameter status: A value indicating the response status (1 for failure, 0 for success).
func setNetworkNameResponse(status: UInt8)
/// Delegate method that handles the response after the app sends the SetNetworkKey data to the BLE device.
/// This method is called when the BLE device sends back the set network key data response.
/// The response status indicates whether the operation was successful.
/// - Parameter status: A value indicating the response status (1 for failure, 0 for success).
func setNetworkKeyResponse(status: UInt8)
/// Delegate method that handles the response after the app sends the SetMeshLocalPrefix data to the BLE device.
/// This method is called when the BLE device sends back the set mesh local prefix data response.
/// The response status indicates whether the operation was successful.
/// - Parameter status: A value indicating the response status (1 for failure, 0 for success).
func setMeshLocalPrefixResponse(status: UInt8)
}
Get device
information. Refer to the Figure 1-21 and
Figure 1-22 read the device
information based on the stack type (Thread, MAC, Phy and Zigbee
device).
//fetch software version
m_ZBPeripheral?.command_GetSwVersion()
//fetch device state
m_ZBPeripheral?.command_GetDeviceState()
//fetch mac id
m_ZBPeripheral?.command_GetMacID()
//fetch stack type
m_ZBPeripheral?.command_GetStackType()
//fetch current channel
m_ZBPeripheral?.command_GetCurrentChannel()
//fetch device name
m_ZBPeripheral?.command_GetDeviceName()
Figure 1-21. Device
Information
Figure 1-22.
Device Information Based on Stack Type
Commission and
Provision for Thread, MAC, Phy and Zigbee
device.
//Set Channel Map - Zigbee Device Only
//Initialize a channelMap array with the appropriate number of bytes (supported channel 11 - 26).
//Set the bits in the channelMap array based on the state of the checkboxes.
//Convert the channelMap array to a Data object.
//Pass the Data object to the command_SetChannelMap method.
m_ZBPeripheral?.command_SetChannelMap(channel: Data(channelMap))
//Get Commission Status
m_ZBPeripheral?.command_GetCommissionStatus()
//Start Commission
m_ZBPeripheral?.command_StartCommission()
//Set Current Channel - Thread, MAC, PHY only
m_ZBPeripheral?.command_SetCurrentChannel(id: dataFromHexString(hexString: hexValue))
//Set Pan Id - Thread, MAC, PHY only
m_ZBPeripheral?.command_SetPanID(id: dataFromHexString(hexString: hexString!)) // only 2 hexadecimal value
//Set Current Mask - Thread, MAC, PHY only
m_ZBPeripheral?.command_SetChannelMask(id: dataFromHexString(hexString: hexString!)) // only 4 hexadecimal value
//Set User Parameters - Thread, MAC, PHY only
m_ZBPeripheral?.command_SetUserParameter(id: dataFromHexString(hexString: hexString!)) // only 16 hexadecimal value
//Set Ext Pan Id - Thread only
m_ZBPeripheral?.command_SetExtPanID(id: dataFromHexString(hexString: hexString!)) // only 8 hexadecimal value
//Set Network Name - Thread only
m_ZBPeripheral?.command_SetNetworkName(name: str!) // Maximum 16 characters
//Set Network Key - Thread only
m_ZBPeripheral?.command_SetNetworkKey(id: dataFromHexString(hexString: hexString!)) // only 16 hexadecimal value
//Set Mesh Local - Thread only
m_ZBPeripheral?.command_SetMeshLocalPrefix(id: dataFromHexString(hexString: hexString!)) // only 8 hexadecimal value
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.