1.4.1 Bluetooth® Low Energy UART Framework Integration and Usage
Download the framework from the following link: MBD_Framework_v2.1.0
- Import the framework:
- Open Xcode and create a simple project.
- In the project navigator, open the project settings.
- Select the target, and then open the "General" tab.
- Navigate to Frameworks>Libraries>Embedded Content settings.
- Add
"MchpBLELib.xcframework."
Figure 1-23. Import Framework to Project
- First, import the
MchpBLELiblibrary and conform to theBleUARTDelegateprotocol in theViewController. This protocol defines several delegate methods that must be implemented to handle Bluetooth Low Energy events.import MchpBLELib class ViewController: UIViewController, BleUARTDelegate { func bleConnecting(bleScanState:Bool, discoveredPeripherals:[Any]){} func bleDidConnect(peripheralName: String) {} func bleDidDisconnect(error: String) {} func bleDidUpdateStatus(status: String) {} func didWriteRawData(data: Data) {} func didUpdateRawData(data: Data) {} func bleThroughputUpdate(Downlink: String?, Uplink: String?) {} func didEnableRemoteControlMode() {} } - Initialization: Initialize the
BleUARTobject and set its delegate to yourViewController. This is typically done in theviewDidLoadmethod.var bleUart : BleUART? override func viewDidLoad() { super.viewDidLoad() if bleUart == nil{ bleUart = BleUART.sharedInstance(option: .Normal) bleUart.delegate = self } } - Scanning the Devices: To scan
for Bluetooth Low Energy devices, call the
bleScanmethod on theBleUARTobject. Specify a scan timeout, scan configuration, and a filter to narrow down the devices of interest./** Scans for BLE peripheral with a timer. If timeout, stop scanning the peripherals - parameter scanTimeout: BLE scan time. default is 60 seconds - parameter scanConfig: Scan option - parameter filter: BLE scanner wil use this to filter advertising packets. The list of filtered devices is return by the bleUARTDelegate bleConnecting method - returns: None */ self.bleUart?.bleScan(scanTimeout: 10,filter: [.FilterBySpecificString:self.DeviceFilter!]) - When the
bleUartControllerdiscovers a peripheral, it calls thebleConnecting(bleScanState:discoveredPeripherals:)method of its delegate object.typealias peripheralInfo = (String, NSNumber) func bleConnecting(bleScanState:Bool, discoveredPeripherals:[Any]){ for peripheral in discoveredPeripherals{ if peripheral is peripheralInfo{ let peripheralInfo = peripheral as! peripheralInfo print("peripheral name & rssi = \(peripheralInfo)") } } } - Connecting the Device: Once
the Bluetooth Low Energy is connected,
bleUartControllercalls thebleDidConnect(peripheralName:)method of its delegate object.bleUart?.bleConnect(deviceName: "BLE_UART_XXXX") func bleDidConnect(peripheralName: String) { print("callback: bleDidConnect. \(peripheralName)") } - Disconnecting the Device: To
disconnect from a Bluetooth Low Energy device, call the
bleDisconnectmethod on theBleUARTobject with the device's UUID.bleUart?.bleDisconnect(peripheralUUID: "9BCE-XXXX-XXXX-XYXY....") -
Data exchange:
-
Sending Data: The application sends a text file (for example,
500.txt). -
Receiving Data: The
bleUartControllercalls thedidUpdateRawData(data:)method of its delegate object. - To send data to the
Bluetooth Low Energy device, use the
BurstTransmitmethod for Burst Transmission or theTransmitDatamethod for regular data transmission.- Burst
Transmission:
func WriteData() { let bundle = Bundle.main let fileUrl = bundle.url(forResource: "500k", withExtension: "txt") if (fileUrl != nil) { /// BLE UART burst transmission /// /// - Parameters: /// - peripheralUUID: The UUID of the target peripheral /// - profile: BLE UART transparent profile. TRP or TRCBP /// - mode: Operation mode. UART,Checksum,Loopback,FixedPattern /// - fileurl: The URL of BLE UART test file. 10k.txt,100k.txt,200k.txt,500k.txt /// - completion: completion handler is called with the execution result and an optional error bleUart?.BurstTransmit(profile: .TRP, mode: .go_through_uart, fileurl: fileUrl!, completion: {(error) in if error != nil { print("error = \(error!)") } else { print("Burst Transmit Complete.") } } } } func didUpdateRawData(data: Data) {} - Regular
Transmission:
/** BLE UART data transmission - parameter peripheralUUID: UUID of the target peripheral - parameter profile: BLE UART transparent profile. TRP or TRCBP - parameter mode: Operation mode. UART or Loopback mode - parameter data: Data to be send - parameters: - completion: completion handler is called with the execution result and an optional error */ bleUart?.TransmitData(profile: .TRP, mode: ble_uart_mode, data: dat, completion: { [self] error in if(error != nil){ print("Fail, error = \(error!)") }else{} ) - Cancel
Transmission:
/// Cancel the data transmission /// - Parameter peripheralUUID: The UUID of the target peripheral bleUart?.CancelTransmission()
- Burst
Transmission:
-
- Changing Transparent
Profile:
/** Change the BLE UART transparent profile - parameter peripheralUUID: The UUID of the target peripheral - parameter profile: BLE UART transparent profile. TRP or TRCBP - completion: completion handler is called with the execution result and an optional error */ bleUart?.ChangeProfile(peripheralUUID: deviceUUID, profile: .TRP, completion: { error in if(error != nil){ print("Error") } })