3.2.1 Standard Communication Target Connection
Important: Refer to the data sheet for the device you are using as well as the
application notes and the specific interface for additional information and
diagrams.
Using the RJ-11 connector, the MPLAB ICD 4 In-Circuit Debugger is connected to the target device with the modular interface (six conductor) cable. The pin numbering for the connector is shown from the bottom of the target PCB in the figure below.
Important: Cable connections on the debugger and target are
mirror images of each other, that is, pin 1 on one end of the cable is connected to pin
6 on the other end of the cable. See Modular Cable Specification.