5.3.3 How to Use the Hardware Tool Emergency Boot Firmware Recovery Utility
CAUTION:
Only use this utility to restore hardware tool boot firmware to its factory state. Use
only if your hardware tool no longer functions on any machine.
The debugger may need to be forced into recovery boot mode (reprogrammed) in
rare situations; for example, if any of the following occurs when the debugger is connected
to the computer:
- If the debugger has no LEDs lit.
- If the LEDs are cyan in color.
- If the procedure described in How to Invoke the Bootload Mode was not successful.
Important: YOU MUST USE MPLAB X IDE V4.15 OR GREATER TO USE THE EMERGENCY RECOVERY
UTILITY.
Carefully follow the instructions found in MPLAB X IDE under the main menu options Debug > Hardware Tool Emergency Boot Firmware Recovery.

If the procedure was successful, the recovery wizard displays a success screen. The MPLAB ICD 4 will now be operational and able to communicate with the MPLAB X IDE. If the procedure failed, try it again. If it fails a second time, contact Microchip Support at support.microchip.com.