14.3.2 AES-256-CMAC Authentication (AUTH_TYPE = 0)

In AES-256-CMAC Authentication mode, the 128-bit signature of the user application is computed using the AES-256-CMAC algorithm, hence using the 256-bit secret key, AES_256_CMAC_KEY, stored in USB0 page 0.

The computed signature is compared to the signature appended to the 128-bit aligned user application in Flash. The ROM code locates the position of the signature in Flash reading the 8th vector in the ARM Cortex-M4 exception table read from 0x01000000 address. Indeed, this 32-bit word, in little endian format, is written with the size in bytes of the 128-bit aligned user application size plus the 16 bytes of the 128-bit AES-CMAC signature.

Table 14-3. User Application in Internal Flash at 0x01000000
Byte OffsetBits[127:96]Bits[95:64]Bits[63:32]Bits[31:0]
0x000Hard FaultNMIResetStack Pointer
0x010(User App + Signature) SizeUsage FaultBus FaultMem Manage
0x020
0x040
…
User App Size128-bit AES-256-CMAC signature
(User App + Signature) Size

As an example, for a 1000-byte unsigned user application, the size of the 128-bit aligned user application is ((1000 + 16 -1) / 16) * 16 = 1008. Then the User App Size written into the 8th vector is 1008 + 16 = 1024.