The --edf=file
option is mainly used by the
command-line driver, xc8-cc
, to specify the path of the message
description file. The default file is located in the dat directory
in the compiler’s installation directory.
See Compiler Messages for full information about the compiler’s messaging system.