The following sections describe the menu entries. (See the previous section, EEPROM Configuration Tool Installation, and Figure 1 for details on the file menu entries.)
The following figure illustrates the Edit menu with the following entries:
- Copy Service Settings and Paste
Service Settings entries – Allows the duplication of settings among the five
service settings. The Copy Service Settings copies all settings for one
service.
- The Copy Path Settings and Paste Path Settings entries – Allows the duplication
of settings for the RX and TX settings for paths A and B among the
services.
- Preferences – Allows the default
configuration file location and export directory to be set.
Figure 1. Edit Menu Entry
The following figure illustrates the Product menu with the following entries:
- For automotive applications – The
ATA5831/2/3 transceiver family and the ATA5781/2/3/5 receiver family
- For industrial applications – The
ATA8510/5 transceiver family and the ATA8210/5 receiver family
Note: Selecting the receiver family
deactivates all the TX-related settings in the tabs but does not change the
configuration content.
Figure 2. Product Menu Entry
The following figure illustrates the entries of the View menu. The EEPROM Registers entry
opens a separate window (see Figure 4) that
allows the user to directly modify the EEPROM bits. Inside this window, the user can
directly modify the EEPROM bits. When modifying the bits of reserved locations, there is
no modification of the settings in the other tabs of the EEPROM configuration tool.
The Register Diff Tool entry opens a separate window (see Figure 5) that highlights the differences between the current EEPROM settings
and predefined reference settings.
Figure 3. View Menu Entry
Figure 4. EEPROM Register Lister View
The Refresh button restores the latest values in this window. The other tabs do
not display any bit changes in this window. Click save_this_to_hex-file button to
store any changes.
The following figure illustrates the differences between the two settings.
Figure 5. EEPROM Register Difference View
There are two possibilities to check for changes:
- Show Changes vs Reference
– Click the Show Changes vs Reference or Show Changes button to
refresh the configuration in the EEprom Register Diff Tool. Now, click
the vertical ^ button to move the current settings to the “Reference”
column. Click the Show Changes vs Reference button to compare the actual
configuration to the “Reference” values. The differences are highlighted when
scrolling down inside the window. This gives a quick overview of the changes in
two different EEPROM configurations.
- Show Changes – Click the
Show Changes button to get a quick overview of the changes in two
different EEPROM configurations.
Note: Click the > button
between “Bit7 .. 0” and “Reference” to set the reference.