Figure 1 illustrates the IO Ports tab. It configures the IO port B and port C pins of the AVR microcontroller. The configuration of the pin direction and other features are only valid at start-up after a reset. These settings are configurable during run-time by the ROM firmware or the Flash application program.
The IO Ports tab allows the following pin settings:
The alternate settings for these pins mentioned in parentheses are controlled in the other related tabs and overwrite the port settings during run-time. In addition, the status window displays comments on pin usage.