The following are the sequence of steps for setting up an EEPROM
configuration:
- 1.Load the default configuration. For more
details, refer to EEPROM Configuration Tool Installation.
- 2.Modify the EEPROM configuration according
to the application requirements, such as RF, Data Rate (DR), coding, pattern and
more.
- 3.Store the new configuration in a
.xml
file format for later reload into the EEPROM configuration tool.
For programming purposes, store the configuration in a .hex
file format
or any of the other available formats.