Figure 1 illustrates the Services tab for configuring each of the five services for the RX mode, and Figure 4 illustrates the TX mode. These settings are independent of each other. The EEPROM contains Service 0, Service 1 and Service 2, whereas, the SRAM contains Service 3 and Service 4.
Each service is divided into the following sections:
The Services (2) tab continues the Service Settings for the RX mode along with the General Setting for the ID Check Configuration common to all services: