8-bit AVR Microcontroller

Using the TWI

The AVR TWI is byte-oriented and interrupt based. Interrupts are issued after all bus events, like reception of a byte or transmission of a START condition. Because the TWI is interrupt-based, the application software is free to carry on other operations during a TWI byte transfer. Note that the TWI Interrupt Enable (TWIE) bit in TWCR together with the Global Interrupt Enable bit in SREG allow the application to decide whether or not assertion of the TWINT Flag should generate an interrupt request. If the TWIE bit is cleared, the application must poll the TWINT Flag in order to detect actions on the TWI bus.

When the TWINT Flag is asserted, the TWI has finished an operation and awaits application response. In this case, the TWI Status Register (TWSR) contains a value indicating the current state of the TWI bus. The application software can then decide how the TWI should behave in the next TWI bus cycle by manipulating the TWCR and TWDR Registers.

The following figure is a simple example of how the application can interface to the TWI hardware. In this example, a Master wishes to transmit a single data byte to a Slave. This description is quite abstract, a more detailed explanation follows later in this section. A simple code example implementing the desired behavior is also presented.

Figure 1. Interfacing the Application to the TWI in a Typical Transmission
  1. 1. The first step in a TWI transmission is to transmit a START condition. This is done by writing a specific value into TWCR, instructing the TWI hardware to transmit a START condition. Which value to write is described later on. However, it is important that the TWINT bit is set in the value written. Writing a one to TWINT clears the flag. The TWI will not start any operation as long as the TWINT bit in TWCR is set. Immediately after the application has cleared TWINT, the TWI will initiate transmission of the START condition.
  2. 2.When the START condition has been transmitted, the TWINT Flag in TWCR is set, and TWSR is updated with a status code indicating that the START condition has successfully been sent.
  3. 3.The application software should now examine the value of TWSR, to make sure that the START condition was successfully transmitted. If TWSR indicates otherwise, the application software might take some special action, like calling an error routine. Assuming that the status code is as expected, the application must load SLA+W into TWDR. Remember that TWDR is used both for address and data. After TWDR has been loaded with the desired SLA+W, a specific value must be written to TWCR, instructing the TWI hardware to transmit the SLA+W present in TWDR. Which value to write is described later on. However, it is important that the TWINT bit is set in the value written. Writing a one to TWINT clears the flag. The TWI will not start any operation as long as the TWINT bit in TWCR is set. Immediately after the application has cleared TWINT, the TWI will initiate transmission of the address packet.
  4. 4.When the address packet has been transmitted, the TWINT Flag in TWCR is set, and TWSR is updated with a status code indicating that the address packet has successfully been sent. The status code will also reflect whether a Slave acknowledged the packet or not.
  5. 5.The application software should now examine the value of TWSR, to make sure that the address packet was successfully transmitted, and that the value of the ACK bit was as expected. If TWSR indicates otherwise, the application software might take some special action, like calling an error routine. Assuming that the status code is as expected, the application must load a data packet into TWDR. Subsequently, a specific value must be written to TWCR, instructing the TWI hardware to transmit the data packet present in TWDR. Which value to write is described later on. However, it is important that the TWINT bit is set in the value written. Writing a one to TWINT clears the flag. The TWI will not start any operation as long as the TWINT bit in TWCR is set. Immediately after the application has cleared TWINT, the TWI will initiate transmission of the data packet.
  6. 6.When the data packet has been transmitted, the TWINT Flag in TWCR is set, and TWSR is updated with a status code indicating that the data packet has successfully been sent. The status code will also reflect whether a Slave acknowledged the packet or not.
  7. 7.The application software should now examine the value of TWSR, to make sure that the data packet was successfully transmitted, and that the value of the ACK bit was as expected. If TWSR indicates otherwise, the application software might take some special action, like calling an error routine. Assuming that the status code is as expected, the application must write a specific value to TWCR, instructing the TWI hardware to transmit a STOP condition. Which value to write is described later on. However, it is important that the TWINT bit is set in the value written. Writing a one to TWINT clears the flag. The TWI will not start any operation as long as the TWINT bit in TWCR is set. Immediately after the application has cleared TWINT, the TWI will initiate transmission of the STOP condition. Note that TWINT is NOT set after a STOP condition has been sent.

Even though this example is simple, it shows the principles involved in all TWI transmissions. These can be summarized as follows:

The following table lists assembly and C implementation examples. Note that the code below assumes that several definitions have been made, e.g. by using include-files.

Table 1. Assembly and C Code Example
  Assembly Code Example C Example Comments
1
ldi r16, (1<<TWINT)|(1<<TWSTA)|(1<<TWEN)
out TWCR, r16 
TWCR = (1<<TWINT)|(1<<TWSTA)|(1<<TWEN)
Send START condition
2
wait1:
in r16,TWCR 
sbrs r16,TWINT
rjmp wait1
while (!(TWCR & (1<<TWINT)));
Wait for TWINT Flag set. This indicates that the START condition has been transmitted.
3
in r16,TWSR 
andi r16, 0xF8
cpi r16, START 
brne ERROR
if ((TWSR & 0xF8) != START)
  ERROR();
Check value of TWI Status Register. Mask prescaler bits. If status different from START go to ERROR.
ldi r16, SLA_W 
out TWDR, r16
ldi r16, (1<<TWINT) | (1<<TWEN)
out TWCR, r16 
TWDR = SLA_W;
TWCR = (1<<TWINT) | (1<<TWEN);
Load SLA_W into TWDR Register. Clear TWINT bit in TWCR to start transmission of address.
4
wait2: 
in r16,TWCR 
sbrs r16,TWINT 
rjmp wait2
while (!(TWCR & (1<<TWINT)));
Wait for TWINT Flag set. This indicates that the SLA+W has been transmitted, and ACK/NACK has been received.
5
in r16,TWSR 
andi r16, 0xF8
cpi r16, MT_SLA_ACK 
brne ERROR
if ((TWSR & 0xF8) != MT_SLA_ACK)
  ERROR();
Check value of TWI Status Register. Mask prescaler bits. If status different from MT_SLA_ACK go to ERROR.
ldi r16, DATA
out TWDR, r16
ldi r16, (1<<TWINT) | (1<<TWEN)
out TWCR, r16 
TWDR = DATA;
TWCR = (1<<TWINT) | (1<<TWEN);
Load DATA into TWDR Register. Clear TWINT bit in TWCR to start transmission of data.
6
wait3: 
in r16,TWCR 
sbrs r16,TWINT 
rjmp wait3
while (!(TWCR & (1<<TWINT)));
Wait for TWINT Flag set. This indicates that the DATA has been transmitted, and ACK/NACK has been received.
7
in r16,TWSR 
andi r16, 0xF8
cpi r16, MT_DATA_ACK 
brne ERROR
if ((TWSR & 0xF8) != MT_DATA_ACK)
   ERROR();
Check value of TWI Status Register. Mask prescaler bits. If status different from MT_DATA_ACK go to ERROR.
ldi r16, (1<<TWINT)|(1<<TWEN)| (1<<TWSTO)
out TWCR, r16 
TWCR = (1<<TWINT)|(1<<TWEN)|(1<<TWSTO);
Transmit STOP condition.