The Security register supports byte writes, page writes and partial page writes in the upper 16 bytes of the region. Page writes and partial page writes in the Security register have the same page boundary restrictions and behavior as they do in the EEPROM region (see Page Write).
Writing in the Security register requires beginning the device address byte with
1011b
(Bh), matching the hardware address bits (A2, A1) to the
corresponding value determined by the ordering code of the device (see Table 3 and Table 4) and sending a logic ‘0
’ in the Read/Write Select
bit. The device will ACK this sequence.
Following the device address byte, bits A7 and A6 of the word address byte must be set to
10b
regardless of the intended address being written. Refer to
Table 5 for detailed requirements on these bits. Figure 1 is an example of a byte write operation in
the Security register.
The user-programmable portion of the Security register can be permanently inhibited from future writing with the Lock command. The status of the Lock state can be determined by sending a subset of the Lock command.