This section describes the procedures to run the BM70/71-based demo applications.
Notes:
- There are differences in the
response packet sent by the BM70/71 firmware for the
Read_Local_Specific_Primary_Service (0x3C) command in regard to different
firmware versions. Until the firmware Version 1.11, it follows same pattern, and
in V2.03, the response data packet structure changes. To make the application
compactable with all the firmware versions, the read-back function is modified
with #define Older_Firmware_Versions macro.
- By default, this macro is
commented in the code to make it work with the latest released firmware (2.03 at
time of creation of this document). It is recommended that this macro be
un-commented in the code, if an earlier firmware version is used.