Atmel Studio
How do I Reuse My AVR®
Studio 4 Projects with the Microchip Studio?
- 1.Click the menu File → Import AVR Studio 4 project.
- 2.An “Import AVR Studio 4 Project” dialog will appear.
- 3.Type in the name of your project or browse to the project location by clicking the Browse button of the APFS File location Tab.
- 4.Name the new solution resulting from the conversion of your project in the Solution Folder Tab.
- 5.Click Next.
- 6.Microchip Studio will proceed with the
conversion. Some warnings and errors may show up in the
Summary window depending on the complexity and
specificity of your project.
- 7.Click Finish to access your newly converted project.