You can run a test using either of the following methods:
Entering commands is the preferred method to run a test with MDB. It allows you to interact with the target application as it executes in simulation or on actual hardware. The result of each command is displayed one at a time, so that mistakes are more easily understood and corrected (see “Entering Commands Method”).
The Running a Command File method cannot be used after the MDB has been invoked. The command file is included as a parameter in the command line when invoking the MDB (see “Running a Command File Method”).