8.6 SIGROW - Signature Row

The content of the Signature Row fuses (SIGROW) is pre-programmed and read-only. SIGROW contains information such as device ID, serial number, and calibration values.

All the AVR128DB28/32/48/64 devices have a three-byte device ID that identifies the device. The device ID can be read using the Unified Program and Debug Interface (UPDI), also when a device is locked. The device ID for the AVR128DB28/32/48/64 devices consists of three signature bytes, which is given by the following table.

Table 8-4. Device ID
Device Name Signature Byte Address and Value
0x00 0x01 0x02
AVR128DB28 0x1E 0x97 0x0E
AVR128DB32 0x1E 0x97 0x0D
AVR128DB48 0x1E 0x97 0x0C
AVR128DB64 0x1E 0x97 0x0B