1 Harmony 3 Driver and System Service Application Examples for PIC32MK Family

The following applications are provided to demonstrate the typical or interesting usage models of one or more peripheral libraries.

NameDescription
Console Debug System Service using UARTThis example application demonstrates the UART based console and debug system service
FAT File System using NVM MediaThis application shows an example of implementing a FAT disk in the device internal Flash memory
FAT File System using SDSPI MediaThis application shows an example of using the MPLAB Harmony File System to access and modify the contents of a SD card using the SDSPI driver and the SPI PLIB
FreeRTOS BasicThis example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven
FreeRTOS Task NotificationThis example application is to illustrate the FreeRTOS Task Notification feature which is used as a light weight binary semaphore
I2C Driver Asynchronous - I2C EEPROMThis example application shows how to use the I2C driver in asynchronous mode to perform operations on the EEPROM
I2C Driver Asynchronous - I2C Temp SensorThis example application shows how to use the I2C driver in asynchronous mode to communicate with the MCP9808 I2C based temperature sensor
I2C Driver Synchronous - I2C EEPROMThis example application shows how to use the I2C driver in synchronous mode to perform operations on the EEPROM
I2C EEPROM AT24 Driver - EEPROM Read WriteThis example application shows how to use the AT24 driver to perform read and write operations on AT24 series of EEPROM
SPI Driver Asynchronous - Multi InstanceThis example demonstrates how to use multiple instances of the SPI driver in asynchronous mode to communicate with multiple EEPROMs
SPI Driver Asynchronous - Multi ClientThis example demonstrates how to use single instance of the SPI driver in asynchronous mode to communicate with multiple EEPROMs
SPI Driver Asynchronous - Self Loopback Multi ClientThis example demonstrates how to use the SPI driver in asynchronous mode to achieve self-loop back between multiple clients
SPI Driver Synchronous - Self Loopback Multi ClientThis example demonstrates how to use the SPI driver in synchronous mode to achieve self-loop back between multiple clients in RTOS environment
SPI EEPROM AT25 Driver - EEPROM Read WriteThis example application shows how to use the AT25 driver to perform read and write operations on AT25 series of EEPROM
Time System Service Multi-clientThis example application demonstrates the multi-client system timer functionality
USART Driver Asynchronous - USART EchoThis example echoes the received characters over the console using the USART driver in asynchronous mode
USART Driver Asynchronous - USART Multi InstanceThis example echoes the received characters over the two consoles using the USART driver in asynchronous mode
USART Driver Synchronous - USART EchoThis example echoes the received characters over the console using the USART driver in synchronous mode