1.11 SPI Driver Asynchronous - Multi Client

This example demonstrates how to use single instance of the SPI driver in asynchronous mode to communicate with multiple EEPROMs.

Description

This example write and read data to and from two separate EEPROM connected over the same SPI bus by using the multi client feature of the driver. The example also demonstrates how to setup two different EEPROM transfers at different baud rates.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/driver/spi/async/spi_multi_slave/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
pic32mk_mcj_curiosity_pro.XMPLABX project for PIC32MK MCJ Curiosity Pro Board
pic32mk_mca_curiosity_pro.XMPLABX project for PIC32MK MCA Curiosity Pro Board

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
pic32mk_mcj_curiosity_pro.XPIC32MK MCJ Curiosity Pro Board
pic32mk_mca_curiosity_pro.XPIC32MK MCA Curiosity Pro Board

Setting Up PIC32MK MCJ Curiosity Pro Board

Setting Up PIC32MK MCA Curiosity Pro Board