1.15 SPI EEPROM AT25 Driver - EEPROM Read Write

This example application shows how to use the AT25 driver to perform read and write operations on AT25 series of EEPROM.

Description

This example uses the AT25 driver to communicate with the SPI based AT25 series of external EEPROMs to perform write and read operations in Bare-Metal environment.

Downloading and Building the Application

To clone or download this application from GitHub, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/driver/spi_eeprom/at25/at25_eeprom_read_write/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
pic32mk_gp_db.XMPLAB X project for PIC32MK GP Development Kit
pic32mk_mcj_curiosity_pro.XMPLAB X project for PIC32MK MCJ Curiosity Pro Development Board
pic32mk_mca_curiosity_pro.XMPLAB X project for PIC32MK MCA Curiosity Pro Development Board

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
pic32mk_gp_db.XPIC32MK GP Development Kit
pic32mk_mcj_curiosity_pro.XPIC32MK MCJ Curiosity Pro Development Board
pic32mk_mca_curiosity_pro.XPIC32MK MCA Curiosity Pro Development Board

Setting Up PIC32MK GP Development Kit

  • To run the demo, the following additional hardware is required:
  • Connect micro USB cable to the Debug USB connector (J12) on the board to the computer
  • Install EEPROM 4 Click board onto the J1 click board slot provided on PIC32MK GP Development Kit

Setting Up PIC32MK MCA Curiosity Pro Development Board

  • To run the demo, the following additional hardware is required:
  • Connect micro USB cable to the Debug USB connector (J1) on the board to the computer
  • Install EEPROM 4 Click board onto the mikroBUS connector of the PIC32MK MCA Curiosity Pro Development Board