1.7 I2C Driver Asynchronous - I2C EEPROM
This example application shows how to use the I2C driver in Asynchronous mode to perform operations on the EEPROM.
Description
This example uses the I2C driver in Asynchronous mode to communicate with the EEPROM to perform write and read operations in Bare-Metal environment. This application uses I2C driver to read and write data from an AT24CM02 EEPROM device.
Downloading and Building the Application
To clone or download this application from GitHub, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/driver/i2c/async/i2c_eeprom/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| pic32mk_gp_db.X | MPLAB X project for PIC32MK GP Development Kit |
| pic32mk_mcj_curiosity_pro.X | MPLAB X project for PIC32MK MCJ Curiosity Pro Development Board |
| pic32mk_mcm_curiosity_pro.X | MPLAB X project for PIC32MK MCM Curiosity Pro Development Board |
| pic32mk_mca_curiosity_pro.X | MPLAB X project for PIC32MK MCA Curiosity Pro Development Board |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| pic32mk_gp_db.X | PIC32MK GP Development Kit |
| pic32mk_mcj_curiosity_pro.X | PIC32MK MCJ Curiosity Pro Development Board |
| pic32mk_mcm_curiosity_pro.X | PIC32MK MCM Curiosity Pro Development Board |
| pic32mk_mca_curiosity_pro.X | PIC32MK MCA Curiosity Pro Development Board |
Setting Up PIC32MK GP Development Kit
- To run the demo, the following additional hardware is required:
- Connect micro USB cable to the Debug USB connector (J12) on the board to the computer
- Install the EEPROM 3 Click board onto the mikroBUS socket J8 of PIC32MK GP Development Kit
Setting Up PIC32MK MCJ Curiosity Pro Development Board
- To run the demo, the following additional hardware is required:
- Connect micro USB cable to the Debug USB connector (J1) on the board to the computer
- Install the EEPROM 3 Click board onto the mikroBUS Xplained Pro board
- Connect the mikroBUS Xplained Pro board to the EXT1 header (J501) of the PIC32MK MCJ Curiosity Pro Development Board
Setting Up PIC32MK MCM Curiosity Pro Development Board
- To run the demo, the following additional hardware is required:
- Connect a micro USB cable to the USB DEBUG port J500
- Install the EEPROM 3 Click board onto the mikroBUS socket J300 of PIC32MK MCM Curiosity Pro Development Board
Setting Up PIC32MK MCA Curiosity Pro Development Board
- To run the demo, the following additional hardware is required:
- Connect a micro USB cable to the USB DEBUG port
- Install the EEPROM 3 Click board onto the mikroBUS socket of PIC32MK MCA Curiosity Pro Development Board
Running the Application
- Build and program the application using its IDE.
- The LED is turned ON when the value read from the EEPROM matched with the written value.