1 MPLAB® Harmony 3 CAN Bootloader Application Examples
MPLAB® Harmony 3 is an extension of the MPLAB ecosystem for creating embedded firmware solutions for Microchip 32-bit SAM and PIC® microcontroller and microprocessor devices. Refer to the following links for more information.
This repository contains the MPLAB Harmony 3 CAN Bootloader application examples
Bootloader Library
Refer to the Bootloader Library Help for understanding:
- Bootloader framework
- How the Bootloader library works
- Bootloader library configurations
- Bootloader memory layout
Bootloader Examples
The following applications are provided to demonstrate the CAN Bootloader:
| Name | Description |
|---|---|
| CAN Bootloader | This example application shows how to use the Bootloader Library to bootload an application using CAN/CAN-FD protocol |
| CAN Faile Safe Bootloader | This example application shows how to use the Bootloader Library to bootload an application on device having dual Flash bank feature using CAN-FD protocol |
| MPU CAN Bootloader | This example application shows how to use the Harmony Bootloader to bootload an application from SD/eMMC/NAND/Serial Flash memory and receives new application image using CAN-FD protocol and write it to SD/eMMC/NAND/Serial Flash memory |