1.3 MPU CAN Bootloader
This example application shows how to use the Harmony Bootloader to bootload an application from SD/eMMC/NAND/Serial Flash memory and receives new application image using CAN-FD protocol and write it to SD/eMMC/NAND/Serial Flash memory.
Bootloader Application
This is a bootloader application which resides from:
Bootloader stored into SD/eMMC/NAND/Serial Flash memory
Bootloader executes from DDR memory. AT91Bootstrap loads bootloader from SD/eMMC/NAND/Serial Flash memory to DDR memory and executes it.
It uses CAN peripheral library in non-interrupt mode
It calls the bootloader_Tasks() function which receives application to be programmed into SD/eMMC/NAND/Serial Flash memory over CAN-FD bus. And it loads application image from SD/eMMC/NAND/Serial Flash memory to DDR memory and executes it.
It turns on an LED
Trigger Methods
- It uses the On board Switch as bootloader trigger pin to force enter the bootloader at reset of device
SDCARD Host Application
This is an embedded CAN-FD host application which sends the application image stored in the SD card to the target board over the CAN-FD bus
The user application binary is copied into an SD card and inserted in the SD card connected on the host board

Test Application
This is a test application which resides from:
- Application stored into SD/eMMC/NAND/Serial Flash memory
It will be loaded from SD/eMMC/NAND/Serial Flash memory to DDR memory by bootloader application and starts application execution
It blinks an LED and provides console output
Development Kits
The following table provides links to documentation on how to build and run MPU CAN bootloader on different development kits.