1.4 CAN Bootloader Tools Help

This document describes the usage of CAN bootloader host tools

Downloading the host tools

To clone or download the host tools from Github,go to the bootloader repository and then click Clone button to clone this repo or download as zip file. This content can also be download using content manager by following these instructions

Following host tools are provided to be used with different bootloaders

Host ScriptDescription
btl_app_merge_bin.pyUsed to merge the bootloader binary and application binary
btl_bin_to_c_array.pyUsed to convert the binary file to a C style array containing Hex output