5.2 Example
The following code snippet shows an example on how to configure the High Priority Interrupt vector.
High Priority Interrupt configuration
// io.h includes the device header file with register and vector defines #include <avr/io.h> // interrupt.h contains the ISR related content #include <avr/interrupt.h> void high_priority_interrupt_example(void) { // Set the level 1 interrupt vector CPUINT.LVL1VEC = PORTA_PORT_vect_num; // Enable global interrupts sei(); } ISR(PORTA_PORT_vect){ // This interrupt will have level 1 priority // after the configuration in CPUINT.LVL1VEC. // Check if a level 0 ISR has been interrupted if (CPUINT.STATUS & CPUINT_LVL0EX_bm) { } }