1.3.2 Warnings
Read the following warnings before using the Midspan unit:
- Connect the PD-9501GS only to the IP device with which it was bought. Using the PD-9501GS with other IP devices can cause damage to the IP device.
- Read the installation instructions before connecting the PD-9501GS to its power source
- Follow basic electricity safety measures whenever connecting the PD-9501GS to its power source
- A voltage mismatch can cause equipment damage and may pose a fire hazard. If the voltage indicated on the label is different from the power outlet voltage, do not connect the PD-9501GS to that power outlet.