4 Pinout and Packaging
Each pin is controlled by the I/O Pin Controller (PORT) as a general purpose I/O and alternatively can be assigned to one of the peripheral functions: A, B, C, D, E, F, G, H, I, J, K, L, M, or N.
The following tables describe the peripheral signals multiplexed to the PORT I/O pins for each package.
Refer to the I/O PINMUX tables for the list per package of pins powered by AVDD.
Note: The IOSET configurations for the concerned digital alternate output functions must also be considered.
The column “Reset State” indicates the reset state of the line with mnemonics:
- I/O or Peripheral Function – Indicates whether the I/O pin resets in I/O mode or in peripheral function mode.
- I/O/Hi-Z – Indicates whether the I/O is configured as an input, output, or is tri-stated.
- PU/PD – Indicates whether pull up, pull down, or nothing is enabled.