2.2.3.2 BL_BootCommandProcess()

bl_result_t BL_BootCommandProcess (uint8_t * commandBuffer, uint16_t commandLength)

Executes the required action based on the block type received in the bootloader data buffer.

Parameters:
in commandBuffer

- Pointer to the start of the bootloader operational data

in commandLength

- Length of the new data received by the FTP

Returns:

BL_PASS - Process cycle finished successfully

BL_FAIL - Process cycle failed unexpectedly

BL_ERROR_UNKNOWN_COMMAND - Process cycle encountered an unknown command

BL_ERROR_VERIFICATION_FAIL - Process cycle failed to verify the application image

BL_ERROR_COMMAND_PROCESSING - Process cycle failed due to a data or processing related issue

BL_ERROR_ADDRESS_OUT_OF_RANGE - Process cycle failed due to an incorrect address