4.2.1 qmm_queue_init Function

C

void qmm_queue_init(queue_t *q, uint8_t capacity)

Summary

Initializes the queue

Description

This function initializes the queue. Note that this function should be called before invoking any other functionality of QMM.

Precondition

None

Parameters

ParamDescription
qThe queue which should be initialized
capacityQueue length (Max No of buffers which can be accomodated in the queue)

Returns

None.

Example

queue_t app_queue;
uint8_t queue_size = 10;
qmm_queue_init(&app_queue, queue_size);

Remarks

None