6.7.7 imaxdiv Function
Compute division and remainder of a greatest-width integer in one operation.
Include
<inttypes.h>
Prototype
imaxdiv_t imaxdiv(intmax_t numer, intmax_t denom);
Arguments
numer- The numerator argument
denom- The denominator argument
Return Value
The imaxdiv function computes the division, numer /
denom, and remainder, numer % denom, of the arguments and
returns the results in an imaxdiv_t structure.
Remarks
If either part of the result cannot be represented, the behavior is undefined.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <inttypes.h>
#include <stdio.h>
int main(void)
{
intmax_t numer, denom;
imaxdiv_t result;
numer = 400;
denom = 3;
result = imaxdiv(numer, denom);
printf("The remainder of %" PRIdMAX " divided by %" PRIdMAX " is %" PRIdMAX "\n", numer, denom, result.rem);
}
Example Output
The remainder of 400 divided by 3 is 1