6.16.5 offsetof Macro
Gives the offset of a structure member from the beginning of the structure.
Include
<stddef.h>
Prototype
size_t offsetof(type
T, member-designator
mbr)
Arguments
T- the type of the structure
mbr- the name of the member in the structure
T
Return Value
Returns the offset in bytes of the specified member (mbr) from the
beginning of the structure with type size_t.
Remarks
This macro is particularly useful since the MPLAB XC16, XC-DSC, and XC32 compilers
word-align structure members, so the member offsets are not based purely on the member
sizes. Additionally, the word size used for alignment varies between compiler and
device. Structures can also be packed using for example the packed
attribute or compiler options, which might also alter the offsets of the structure
members. The MPLAB XC8 compiler, however, does not align members within structures.
The macro offsetof is undefined for bit-fields. An error
message will occur if bit-fields are used.
When building for PIC devices with MPLAB XC8, the expression represented by this macro is evaluated at runtime, hence it does not represent a constant expression and cannot be used where a constant expression is required. For other devices, this macro represents a constant expression.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <stddef.h>
#include <stdio.h>
struct info {
char item1[5];
int item2;
char item3;
float item4;
};
int main(void)
{
printf("Offset of item1 = %d\n", offsetof(struct info, item1));
printf("Offset of item2 = %d\n", offsetof(struct info, item2));
printf("Offset of item3 = %d\n", offsetof(struct info, item3));
printf("Offset of item4 = %d\n", offsetof(struct info, item4));
}
Example Output
Offset of item1 = 0
Offset of item2 = 6
Offset of item3 = 8
Offset of item4 = 10
Example Explanation
In the above example, which shows typical output for the MPLAB XC16 compiler, although
item1 is only 5 bytes wide (char item1[5]),
padding had been added by the compiler, so the address of item2 is
aligned on an even (16-bit) boundary. The same occurs with item3; it is
1 byte wide (char item3) with 1 byte of padding. Different values would
be printed if the structure was packed.