6.4.1 Implementation-defined Error Conditions
The following are error condition macros in addition to those specified by the C language
specification that might be assigned to errno by the Microchip Unified
Standard Library. They expand to positive integer constant expressions with type int,
suitable for use in #if preprocessing directives
| Macro | Error condition |
|---|---|
E2BIG | Argument list too long |
EACCES | Permission denied |
EADDRINUSE | Address already in use |
EADDRNOTAVAIL | Address not available |
EADV | Advertise error |
EAFNOSUPPORT | Address family not supported by protocol family |
EAGAIN | No more processes |
EALREADY | Socket already connected |
EBADE | Invalid exchange |
EBADF | Bad file number |
EBADFD | File descriptor invalid for this operation |
EBADMSG | Bad message |
EBADR | Invalid request descriptor |
EBADRQC | Invalid request code |
EBADSLT | Invalid slot |
EBFONT | Bad font file fmt |
EBUSY | Device or resource busy |
ECANCELED | Operation canceled |
ECHILD | No children |
ECHRNG | Channel number out of range |
ECOMM | Communication error on send |
ECONNABORTED | Software caused connection abort |
ECONNREFUSED | Connection refused |
ECONNRESET | Connection reset by peer |
EDEADLK | Deadlock |
EDEADLOCK | File locking deadlock error |
EDESTADDRREQ | Destination address required |
EDOTDOT | Cross mount point (not really error) |
EDQUOT | Disc quota exceeded |
EEXIST | File exists |
EFAULT | Bad address |
EFBIG | File too large |
EHOSTDOWN | Host is down |
EHOSTUNREACH | Host is unreachable |
EHWPOISON | Memory page has hardware error |
EIDRM | Identifier removed |
EINPROGRESS | Connection already in progress |
EINTR | Interrupted system call |
EINVAL | Invalid argument |
EIO | I/O error |
EISCONN | Socket is already connected |
EISDIR | Is a directory |
EISNAM | Is a named type file |
EKEYEXPIRED | Key has expired |
EKEYREJECTED | Key was rejected by service |
EKEYREVOKED | Key has been revoked |
EL2HLT | Level 2 halted |
EL2NSYNC | Level 2 not synchronized |
EL3HLT | Level 3 halted |
EL3RST | Level 3 reset |
ELIBACC | Can't access a needed shared lib |
ELIBBAD | Accessing a corrupted shared lib |
ELIBEXEC | Attempting to exec a shared library |
ELIBMAX | Attempting to link in too many libs |
ELIBSCN | .lib section in a.out
corrupted |
ELNRNG | Link number out of range |
ELOOP | Too many symbolic links |
EL3RST | Level 3 reset |
EMEDIUMTYPE | Wrong medium type |
EMFILE | File descriptor value too large |
EMLINK | Too many links |
EMSGSIZE | Message too long |
EMULTIHOP | Multihop attempted |
ENAMETOOLONG | File or path name too long |
ENAVAIL | No XENIX semaphores available |
ENETDOWN | Network interface is not configured |
ENETRESET | Connection aborted by network |
ENETUNREACH | Network is unreachable |
ENFILE | Too many open files in system |
ENOANO | No anode |
ENOBUFS | No buffer space available |
ENOCSI | No CSI structure available |
ENODATA | No data (for no delay io) |
ENODEV | No such device |
ENOENT | No such file or directory |
ENOEXEC | Exec format error |
ENOKEY | Required key not available |
ENOLCK | No lock |
ENOLINK | Virtual circuit is gone |
ENOMEDIUM | No medium found |
ENOMEM | Not enough space |
ENOMSG | No message of desired type |
ENONET | Machine is not on the network |
ENOPKG | Package not installed |
ENOPROTOOPT | Protocol not available |
ENOSPC | No space left on device |
ENOSR | No stream resources |
ENOSTR | Not a stream |
ENOSYS | Function not implemented |
ENOTBLK | Block device required |
ENOTCONN | Socket is not connected |
ENOTDIR | Not a directory |
ENOTEMPTY | Directory not empty |
ENOTNAM | Not a XENIX named type file |
ENOTRECOVERABLE | State not recoverable |
ENOTSOCK | Socket operation on non-socket |
ENOTSUP | Not supported |
ENOTTY | Not a character device |
ENOTUNIQ | Given log. name not unique |
ENXIO | No such device or address |
EOPNOTSUPP | Operation not supported on socket |
EOVERFLOW | Value too large for defined data type |
EOWNERDEAD | Previous owner died |
EPERM | Not owner |
EPFNOSUPPORT | Protocol family not supported |
EPIPE | Broken pipe |
EPROTO | Protocol error |
EPROTONOSUPPORT | Unknown protocol |
EPROTOTYPE | Protocol wrong type for socket |
EREMCHG | Remote address changed |
EREMOTE | The object is remote |
EREMOTEIO | Remote I/O error |
ERESTART | Interrupted system call should be restarted |
ERFKILL | Operation not possible due to RF-kill |
EROFS | Read-only file system |
ESHUTDOWN | Can't send after socket shutdown |
ESOCKTNOSUPPORT | Socket type not supported |
ESPIPE | Illegal seek |
ESRCH | No such process |
ESRMNT | Srmount error |
ESTALE | Stale file handle |
ESTRPIPE | Streams pipe error |
ETIME | Stream ioctl timeout |
ETIMEDOUT | Connection timed out |
ETOOMANYREFS | Too many references: cannot splice |
ETXTBSY | Text file busy |
EUCLEAN | Structure needs cleaning |
EUNATCH | Protocol driver not attached |
EUSERS | Too many users |
EWOULDBLOCK | Operation would block |
EXDEV | Cross-device link |
EXFULL | Exchange full |