6.1.1 NDEBUG Macro
A macro used by <assert.h> to specify the operation of
certain debugging features.
Value
This macro is not defined by <assert.h> and must be defined
by the user.
Remarks
NDEBUG must be defined as a macro by the user if and when required. Use
the #define preprocessor directive to define the macro. It does not
need to define any replacement string.
If the macro is defined at the point where <assert.h> is included, it
disables certain debugging functionality of the header content supplied by that
inclusion, in particular, the assert() macro (assert Macro). The
NDEBUG macro may be undefined to allow
<assert.h> to be included in subsequent code and with the full
debugging functionality provided.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
int main(void)
{
int a;
a = 4;
#define NDEBUG /* negate debugging - disable assert() functionality */
#include <assert.h>
assert(a == 6); /* no action performed, even though expression is false */
#undef NDEBUG /* ensure assert() is active */
#include <assert.h>
a = 7;
assert(a == 7); /* true - no action performed */
assert(a == 8); /* false - print message and abort */
}
Example Output
sampassert.c:14 a == 8 -- assertion failed
ABRT