6.14.3 va_copy Macro
Copies a va_list object.
Include
<stdarg.h>
Prototype
void va_copy(va_list dest, va_list src);
Arguments
dest- the
va_listobject to be initialized src- the
va_listobject to copy
Remarks
The function copies the src object into dest, such that
the state of dest will reflect any call made to
va_start to intialize src as well as the same
sequence of va_arg macro calls that modified src.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <stdio.h>
#include <stdarg.h>
#include <limits.h>
/* print values as a percentage of the maximum value
* list ends with 0 value
*/
void PrintAsPercent(int first, ...)
{
char * buffer;
int val = first;
int valMax = INT_MIN;
va_list vl_parse, vl_print;
va_start(vl_parse, first);
/* copy, after having called va_start */
va_copy(vl_print, vl_parse);
/* find the largest value */
while(val != 0) {
val = va_arg(vl_parse, int);
if(val > valMax)
valMax = val;
}
va_end(vl_parse);
/* va_start not necessary with va_print */
val = first;
while(val != 0) {
printf("%d%% ", val*100/valMax);
val = va_arg(vl_print, int);
}
va_end(vl_print);
printf("\n");
}
int main(void)
{
PrintAsPercent(10, 23, 156, 42, 88, 0);
}
Example Output
6% 14% 100% 26% 56%