2.1 NVM-Nonvolatile Memory Module (Writing to DFM)
In Section 10.4.2 Writing to DFM, the stepwise process is clarified to provide specific instructions on when to enable interrupts during the NVM Write sequence. The code example in Example 10-10 is also amended with an additional line. The changes are shown below in bold.
- Set NVMADR registers with the target byte address.
- Load NVMDATL register with desired byte.
- Set the NVMCMD control bits to
‘b011(Byte Write). - Disable all interrupts.
- Perform the unlock sequence as described in the Unlock Sequence section.
- Set the GO bit to start the DFM byte write.
- Interrupts can be enabled after the GO bit is set. If it is not desired to have interrupts during DFM write, then enable interrupts after the next step when the GO bit is cleared.
- Monitor the GO bit or NVMIF interrupt flag to determine when the write has been completed.
- Set the NVMCMD control bits to
‘b000.
Example 10-10. Writing a Byte to Data Flash Memory in
C
// Code sequence to write one byte to a DFM // DFM target address is specified by DFM_ADDR // Target data are specified by ByteValue // Save interrupt enable bit value uint8_t GIEBitValue = INTCON0bits.GIE; // Load NVMADR with the target address of the byte NVMADR = DFM_ADDR; NVMDATL = ByteValue; // Load NVMDAT with the desired value NVMCON1bits.CMD = 0x03; // Set the byte write command INTCON0bits.GIE = 0; // Disable interrupts //––––––––– Required Unlock Sequence ––––––––– NVMLOCK = 0x55; NVMLOCK = 0xAA; NVMCON0bits.GO = 1; // Start byte write //––––––––––––––––––––––––––––––––––––––––––––––– INTCON0bits.GIE = GIEBitValue; // Restore interrupt enable bit value (if interrupts are desired during DFM write) while (NVMCON0bits.GO); // Wait for the write operation to complete // Verify byte write operation success and call the recovery function if needed if (NVMCON1bits.WRERR){ WRITE_FAULT_RECOVERY(); } NVMCON1bits.CMD = 0; // Disable writes to memory