37.3.3.2 STS - Store Data to Data Space Using Direct
        Addressing
The STS instruction is used to store data that are shifted serially into
            the PHY layer shift register to the system bus address space. The STS
            instruction is based on direct addressing, and the address must be given as an operand
            to the instruction for the data transfer to start. The address is the first set of
            operands, and data are the second set. The size of the address and data operands is
            given by the size fields presented in Figure 37-9.
            The maximum size for both address and data is 32 bits.
The STS supports repeated memory access when combined with
            the REPEAT instruction.
STS Instruction
                OperationSTS instruction is depicted in Figure 37-9, following this sequence: - The address is sent.
 - An Acknowledge (ACK) is sent back from the UPDI if the transfer was successful.
 - The number of bytes, as specified
                    in the 
STSinstruction, is sent. - A new ACK is received after the data have been successfully transferred.