4.2 Hardware Installation

The following section describes the hardware installation instructions for the PD-9601GCI/DC PoE Midspan.

  1. Connect an Ethernet cable from the desired source network device (that is, computer, router, switch, and so on) to the DATA IN RJ45 connector of the PD-9601GCI/DC unit.
  2. Connect the terminal block power source(s) to the PD-9601GCI/DC unit.
  3. Connect an RJ45 terminated Ethernet cable to the DATA & POWER OUT connector on the PD-9601GCI/DC unit. Connect the other end of the cable to a compatible PD device. See the following figure for an example.
  4. Verify that the Ethernet cable length is less than 100m from the Ethernet source to the load/remote terminal.
Figure 4-2. Hardware Installation