1.4.5 IOC Without a Timer
| Modules | Limit High | Resolution |
|---|---|---|
| IOC/INT | 4.194 s | 5.5 μs |
This method uses the IOC feature to increment a single register instead of a timer.
OVERVIEW
Without a timer, the microcontroller must spend its time polling and incrementing registers. This forces the CPU to be stuck inside of the software routine until the duty cycle is finished being measured. Refer to Figure 2 for a picture of what is being measured.
SETUP
After executing the setup in section IOC Without a Timer, the duty cycle percentage can be calculated by using Figure 1.
LIMITATIONS
This is the same resolution as the pulse measurements. The uncertainty is plus or minus two clock periods.