2 Demo Requirements
| Requirement | Description |
|---|---|
| Hardware and Accessories | |
| PolarFire® ESB | MPF200-ETH-SENSOR-BRIDGE |
| NVIDIA® Jetson AGX Orin™ Developer Kit1 | A MIPI CSI-2 camera is attached to the sensor bridge and connected to the AGX Orin Devkit through Ethernet. This kit has to be bought separately. |
| One MIPI CSI-2 camera module | IMX477-based Arducam camera module is included in the kit |
| One 10G Ethernet cable | Included in the kit |
| SFP+ to RJ45 converter | Included in the kit |
| 12V/5A power supply | Included in the kit |
| Monitor with DisplayPort input | Display for the AGX Orin Devkit |
| Keyboard and mouse | Required to configure the AGX Orin Devkit. |
Note: The Quick Start Guide provides setup instructions for use with a Jetson Orin AGX Developer Kit. If you are using an IGX Developer Kit, follow the specific steps intended for the IGX kit. We highlight the sections where instructions differ for each kit.