1 Harmony 3 Driver and System Service Application Examples for SAM L10/L11 Family
The following applications are provided to demonstrate the typical or interesting usage
models of one or more drivers, system services and RTOS.
Name | Description |
---|---|
Console Debug System Service using UART | This example application demonstrates the UART based console and debug system service |
FreeRTOS Basic | This example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven |
I2C Driver Asynchronous - I2C EEPROM | This example application shows how to use the I2C driver in asynchronous mode to perform operations on the EEPROM |
I2C Driver Asynchronous - I2C Multi-client | This example application shows how to use multi-client feature of the I2C driver in asynchronous mode to communicate with temperature sensor and an EEPROM |
SDSPI Driver Asynchronous - SDSPI Read Write | This example application shows how to use the SDSPI driver in asynchronous mode to perform non-blocking operations on the SD Card Media |
SPI Driver Asynchronous - Multi Client | This example demonstrates how to use single instance of the SPI driver in asynchronous mode to communicate with multiple EEPROMs |
Time System Service Multi-client | This example application demonstrates the multi-client system timer functionality |
TrustZone FreeRTOS Basic | This example application blinks an LED to show the FreeRTOS threads that are running in non-secure mode and to indicate status |
USART Driver Asynchronous - USART Echo | This example echoes the received characters over the console using the USART driver in asynchronous mode |